IoT enabler
Products shown: 1
PR-SC4
The PR-SC4 device is one of the telemetry device that the Prosa Infrastructure uses in order to create an Internet Of Things. In this case, the “Things” are supposed to be the dispenser of beverages and cold room for goods storage. The primary goal of the PR-SC4 device is to communicate to the Prosa system diagnostic parameters and eventually alarms related to the temperatures of the storage equipment. To this aim, the PR-SC4 can work in conjunction with the electronic thermostat of the cooling equipment when available.The PR-SC4 contains a modem and uses Bluetooth and a Machine to Machine (M2M) SIM in order to communicate with the Prosa Infrastructure through the mobile network. The network is also exploited by the PR-SC4 in order to compute a triangulation of the position of the cooling equipment.